| 1 |
Set the compilation options to run your project in Debug or Release modes, and choose if you want to activate the Online Changes |
| 2 |
Compile the application and see all the remaining warnings and errors
|
| 3 |
Connect the KAS to the target device |
| 4 |
Download the Application compiled on the KAS IDE to the target device |
| 5 |
Start / stop the device, and control your application with the script commands |